Hello
We encounter I2C fail issue.
SOC can't not recognize TAS5711.
Please help to solve it.
Thanks,
Edgar
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
We encounter I2C fail issue.
SOC can't not recognize TAS5711.
Please help to solve it.
Thanks,
Edgar
Hi Edgar,
Regards,
Hector Zhang
Hi Hector
1.The pull-up resistors of SCL/SDA were put on SOC side in another page.
2.The 100K pull-up resistor for A_SEL pin was follow TAS5711's EVM schematic.
Is there helpful for this issue if change to 15K?
3.The waveform of SCL/SDA as attachment.
4.I followed the recommand command sequence as page 38 in datasheet, but SOC always can't access TAS5711 via I2C.
But I can access other I2C device via the same I2C bus.
I will try to replace the pull-up resistor from 100K ot 15K on A_SEL.
Thanks,
Edgar
Edgar,
The waveform indicates you are using 0x34 address, but since you pulled up A_SEL, you should use 0x36 instead.
Also, please have a check on A_SEL, PDN and RESET pin after power-up. Thanks.
Regards,
Hector Zhang
Hi Edgar,
I see it is long time no follow up, so i will close this topic now. If there is more feedback, please keep post on this thread.
Dylan