Other Parts Discussed in Thread: TPA3112D1
We want to use for an new produkt the Amplifier TPA3112D1PWPR to drive an 8Ω Horn speaker.
For testings and measurements we bought the EVM but we've got issues with powering it up.
Befor powering up with +24DC:
- set the jumpers: JP1, JP2, JP5.
- SD pin to GND (after power up i've got an high Signal +21VDC)
- 100K resistance betwen AVCC
- 1KHz 800mV on INP
The only output signal I've got is a little swing from 100mV.
Measured on the jumper JP1 i've got an high level from +21VDC.
Sometimes the AMP starts up, when i often plug and unplug the power supply or once i forgot to switch of the Powersupply and after 3 Hours it starts out of nowhere.
When it runs once there are no problems. Then when i switch off the supply for some seconds it will start instantandly with no issues.