Part Number: SIDEGIG-GUITAREVM
Other Parts Discussed in Thread: TPA3255EVM
Hi
Need Help configuring on Both devices a did a Initial Configuration but Audio Output does not output is low.
yes I do start de amplifier in reset and then I'll toggle S1 to normal.
Speaker connected is 150watts 4ohms.
Also If I wanted to use a Bass instead of a Guitar on the SIDEGID what parts do I need to change or playwith.