This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Decoding pulse-code modulated BFSK signals with the Goertzel algorithm

Hello,

I do not have one of the specified chips, but another TI chip in combination with a third party chip. I am here because I hope that someone here can help me understand the concepts a little better.

The third party chip receives a Bell 103 BFSK signal (110 / 300 bps), and forwards the samples on a I2S / PCM bus. The sampling rate is 8 kHz.
What is the best way to determine 1's and 0's from this PCM signal? 

I have looked at the Goertzel algorithm. This seems very promising, but I am starting to doubt that now.
With 8 kHz sampling, so 1 sample per 0.125 ms, this would come down to around 26 samples per 3.33 ms (the time per bit in the 300 bps FSK signal).

If I understood it correctly, the Goertzel algorithm can only achieve a frequency bin width / resolution of 8000 / 26 = ~300 Hz.
This would not be sufficient, as the BFSK mark and space frequencies used in this system are 1070 and 1270 Hz.

I was hoping perhaps someone here could give me hints to tackle this.