Other Parts Discussed in Thread: TAS5630, TAS5630B
Hello All,
The datasheet recommended design and EVM schematic for both the TPA3255 and TAS5630 show a 100 ohm resistor in series with the INPUT_X pins of the IC. In looking through the schematics, EVM manuals, and other application notes we could not find any mention for why these would be required.
We are currently experimenting with an evaluation board in PBTL configuration containing the TAS5630 and made the following observation: The 100 ohm series resistor forms a resistor divider with internal circuitry that attenuates the signal by half. In addition, the DC component of the signal gets set to PVDD/25.5319 (~0.94V for a 24V supply and ~ 1.88V for 48V).
If the internal resistance of the TAS5630 is 33k Ohms, why is the signal attenuating by 2x?
Does putting the IC in PBTL configuration result in the Analog loop filter setting a 200 ohm differential terminator across the A and B inputs?
Will the TPA3255 exhibit this same behavior?
Thank You.