Could I program the TLV320AIC3254EVM-K for PurePath Studio Graphical Development Environment on Win10 system? I couldn't complete the EEPROM Programming and fail to connect the GDE
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Could I program the TLV320AIC3254EVM-K for PurePath Studio Graphical Development Environment on Win10 system? I couldn't complete the EEPROM Programming and fail to connect the GDE
hankun xue,
Unfortunately no, there is an issue with updating the EEPROM when using PPS. if you'd like to update the firmware, please use the GUI instead.
best regards,
-Steve wilson
Hi Steve
Thanks for the reply. Due to some reasons, I have to use PurePath for my design.
How about Win7 system? Could I use WinXP virtual machine on Win10 system to program EEPROM? All I need to do is to download and run my design on the EVM, is there any ways to do that?
Regards
Hankun,
You can still use Purepath for everything else... you just need the GUI to change the EEPROM firmware.
Perhaps I'm misunderstanding you... Is the issue that the AIC3254 is set up for the wrong sampling rate? and you want to change the EEPROM firmware so the USB audio processor runs at a different rate? Or what exactly is the problem?
best regards,
-sTeve Wilson