Other Parts Discussed in Thread: TPS3128,
Hi, I have 3 questions. This is my first time using AMP.
Question 1.
I am going to use one 30W(RMS) Speaker and want to use TPS3128 for the amp.
In this case, do I have to use TPS3128 as PBTL mode? or Mono mode?
.
If I can use mono mode, then can I use TPA3128 as mono mode? Because In the datasheet there says TPA3129 can be used as Mono mode. There are no comments with TPS3128.
.
If then, are Pin setting same?
1. INPR, INNR Directly to Ground.
2. Connect OUTPL, and OUTPL to Speaker?
.
Question 2.
I am going to use 7s Battery. Battery Voltage will be 21V~29V.(28.98 is max voltage).
In the data sheet absolute max rating of PVCC, AVCC is 30V and recommend is 26V.
Can I use battery voltage directly to PVCC, AVCC? Or would you recommend using DCDC Converter to make voltage down?
.
.
Question 3.
What is the meaning of TTL logic levels with compliance to AVCC? I thought TTL Logic means using 5V.
But AVCC is not 5V.
.
Can I make short these MODSEL, SDZ, MUte pins to AVCC?
Thanks.