Other Parts Discussed in Thread: TAS2770
I was wondering if someone could provide some insight on the correct settings in order to receive current sense and voltage sense data in Audacity, using the setup of the Pure Path software, as I am currently unable to receive any data,
Currently, in the Pure Path software under the Receiver tab, I have the word length set to 16 bits and the slot length set to 32 bits (don't know if this is right). Also, I have the left channel time slot set as 0 and the right channel slot set to 2. In the transmitter tab, I selected the bus keeper option and put the I-sense data in slot 0 and the V-sense data in slot 2.
In the Texas Instruments USB Audio Device Control Panel, I set the input as 8-channels, 24 bits and the output as 8-channels, 32 bits.
Under my Windows Sound Control panel, I set the default format for my Microphone as 8 channel, 32 bit, 44100 Hz. I set the default format for my speaker to be 24 bits, 44100 Hz.
Finally, in Audacity, I generated my tone input to the TAS2770 formatted as a Mono, 44.1kHz 24-bit signal. I set my sampling format as a 32 bit float.
I don't really have that much experience with audio devices, so could someone let me know if any of these settings are wrong and what they should be?
Thanks so much!