Hi team,
It is the last issue of the below link. Could you kindly provide some debug direction.
https://e2e.ti.com/support/audio/f/6/p/911258/3371248#3371248
We spend some time to do the test. We also think that it is related with clock structure. Please refer the clock waveform as below.
fMCLK (R18)= 12.288MHz
fI2C_clk (R19)=3.053MHz
fI2C_ws (R21)=48KHz
#2 register setting difference
Register Addr 0x0 = 0x61
Register Addr 0x1 = 0x3
phase delay fail:-58 degree
#3 register setting difference
Register Addr 0x0 = 0x61
Register Addr 0x1 = 0x0
Register Addr 0x2 = 0x49
Register Addr 0x7 = 0x14
phase delay pass:17.96 degree
THD+N Fail : -29.68( Spec>=60dB)
May I know whether there is a setting can pass phase delay and THD+n at same time? Please let me know your recommendation setting and debug flow.
We would like to make the debug flow more efficiency. Thanks.