Other Parts Discussed in Thread: TAS2770
Hi,
I am interested in using the TAS2770 EVM to test a voice coil actuator, in which I will need to send DC voltages/non-audio waveforms to my actuator from the TAS2770 output. Would I be able to do this with the EVM? Would I need to use PPC3, and would PPC3 support this? Is there an API of sorts to interface with the board via USB?
Also, a general question about I2S: can I drive two TAS2770s over a single I2S port (is this how stereo works)? Sorry, I am new to audio and using I2s in applications.
Thanks,
Chris