Other Parts Discussed in Thread: LM4952,
Hi Team,
I am designing a circuit with the LM4952, and I have two questions.
1. About pop noise during shutdown operation
If the shutdown operation is turned OFF → ON or ON → OFF when there is no signal input, will a pop noise occur? (The circuit configuration assumes Figure 2 in the data sheet.)
Also, if it occurs, is there a way to reduce the pop noise?
2. About tantalum capacitors
Data sheet P.13 states that " Do not substitute a ceramic capacitor for the tantalum. Doing so may cause oscillation." Since the use of tantalum capacitors is prohibited, is there any way to replace tantalum capacitors? Although it is a separate device, the following inquiry states that it can be replaced by mounting a resistor in series with the ceramic converter.
https://e2e.ti.com/support/audio/f/6/p/701040/2597783?tisearch=e2e-sitesearch&keymatch=LM4952#2597783
With this device, the same problem can be solved by raising the ESR. Is there no problem in recognition? And what are the recommended values for the resistance in that case?
Beat Regards,
Tom Liu