This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3144D2: Problem for high slew rate /SD and /FAULT

Guru 19655 points
Part Number: TPA3144D2


The maximum rating of TPA3144D2 is described slew rate: 10V/ms, but one customer occur /SD and /FAULT slew rate more than rating: about 13.3V/ms.

Are below operate relation for higher slew rate?

①Output is continuous ON ⇔ OFF, or keep OFF.

②Output volume is smaller than setting value.

③When /SD and /FAULT become high, AMP/Speaker flow large current.

Best regards,

Satoshi