Other Parts Discussed in Thread: OPA227, , DIT4192, OPA1612,
I am currently designing a prototype analog-to-digital converter with a PCM4222 and DIT4192. The analog front end uses OPA1612 input buffers. As recommended in the datasheet, I'm using OPA227 opamps as VREF drivers. In some areas, the overall design is similar to TI's EVM board, in others it's not. Clocking is done using an FPGA. I'm getting 121dB of dynamic range (noise floor with no input signal, 20-22.000 Hz BW) within the audio band which is according to spec but there is a lot of DC on the output which also was reported in this post by another poster.
With the internal HP filter enabled it hovers around -95~105dB on both channels but when the filter is off, I'm getting -69dB on the left and -76dB on the right channel. I even tried to temporarily adjust the DC offset using a trimmer but I was not able to get rid of it. Quite the opposite actually - it got only worse.
Is there something I can look into to remove the DC from the signal?
Also, the datasheet states -108dB THD+N @ -1dBFS - but no matter what I do, the best I can get at -1dBFS are some measly -92dB. These are mostly higher order harmonics. When measuring the actual analog signal after the input buffers (+2dBu at each VIN+ and VIN-), there's no sign of harmonics at all - so it must be the PCM4222 input stage or conversion adding those.
Any ideas?