Other Parts Discussed in Thread: TLV320AIC3254,
Hi Gents,
i'm using the TLV320AIC3254 as a codec between analog mic and speaker and a radio module.
Frames on the I2S interface ( Dout / WCLK / BCLK) so the TLV outputs are from 0 to 3.3V.
Signal from my radio module to the TLV ( module DOUT) are 0-3.3V when not connected to TLV DIN, but drop to 0-500mV when connected, so i've got no audio coming out on the analog side of the TLV.
The TLV is configured as a Master, 16kHz of sampling rate.
I'm using the TLV320AIC3254EVM-K to test the configuration.
I've checked the following :
- Page0 / Register 32, D0 is set to 0 (DIN is used for Audio Data In).
- Page0/Register 54 igot D2-D1 set to 01 (DIN is enabled for Primary Data Input or Digital Microphone Input or General Purpose Clock input)
Can someone assist to understand why the received signal is lowered?
Regards
Bruno