Hello,
I use the LM4766 in single supply mode. For that I use Figure 6 as a bridged amp (Figure 5) in the datasheet.
The resistor RSN and the capacitor CSN left out.
My problem is, the output works very silent (maybe the Spike protection). If I paste the 22uF (Ci) into the ciruit, the output give distortion on the same settings. I can only set the input voltage down so I make a low noise.
If I don't paste Ci, the distortion is less.
In both cases the sound is very silent. Should I change Rf?