This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA2037D1: Impacts of tying EN pin to a voltage greater than VDD+0.3v

Part Number: TPA2037D1

In our design, we have both 3.3V (for MCU/digital) and 2.8V (for audio/analog).  The TPA2037D1 is on the 2.8V LDO but we accidentally tied its "EN" pin to a 3.3V GPIO signal with no voltage divider. That GPIO is driven by another TI part, CC3220.  From the TPA2037D1 datasheet, the "ABSOLUTE MAXIMUM RATINGS" for the "EN"  is VDD+0.3V, so in our case, the maximum allowed would be 3.1V (2.8+0.3). However, it's currently 3.3V so we're exceeding that by 200mV.  Our prototype boards are already made and obviously we will fix this for production, but my questions are:

1. Is this catastrophic and will it cause a device failure ? What are the impacts of this oversight (keeping in mind that these boards are prototypes)?

2. The 3.3V GPIO is controllable and we can limit the current to the minimum setting allowed by the CC3220, would that be of any help? 

3. What is the maximum "RECOMMENDED OPERATING CONDITION" for the EN pin? There isn't any "max" specified in the datasheet, only a min. Would the max recommended value be the same value as the absolute maximum in this case? (ie. VDD+0.3V)  

 

Thanks!
Berry