Part Number: TAS2555YZEVM
Other Parts Discussed in Thread: TAS2563, TAS2557
Hi,
Reading through the PPC User Manual, Appendix B seems to suggest that there is an option to generate header files. I'm guessing this is in the "End System Integration" Block. I only have the options to "Dump the Binary file" and "Tuning and debugging in system" - which seems to want to connect to a debugging device on a smart device. When I go through the "dump" path, I only get these extensions:
- .bin
- .json
- .cfg
What am I missing?
Thanks!