Other Parts Discussed in Thread: SN74LVC1G00
Hi,
Customer of mine is developing 10W spk with LM48511.
the input source is either 3.7V battery of 5V USB
Normally is from battery pack 3.7V
When connected to USB5V, booster will be switched off and direct using USB5V Vin
Need to confirm if I can use NAND Gate to achieve the above operation?