This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3221: The OSCM and OSCP do not have square wave

Part Number: TPA3221


Dear all,

I currently designed a EVM board using TPA3221 chip. The voltage of power is 16V. When I power on, I can not see anything from OSCM (PIN 12) and OSCP (PIN 13).  The Pin 11 is connected to +5V. The schematic circuit is attached. Could you please help to check it. Thank you very much.TPA3221_PA.pdf