This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5760M: Clock Error occurs -> DC Detect Error occurs

Part Number: TAS5760M


Hi all

Would you mind if we ask TAS5760M?

We would like to comfirm the condition that after clock Error occurs DC Detect Error occurs.
(Of course, we recognize that there is no such situation intrinsically.)
In case of clock Error occurring, if the speaker outputXX is more than DCETHRES, does the device operate DC Detect Error?
And then, the customer uses PVDD=24V, will the typ vaule of DCETHRES 5.2V?
Is it correct?

Kind regards,

Hirotaka Matsumoto