This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3106: Codec configuration for Mic to speaker

Part Number: TLV320AIC3106


Hello All,

We have purchased TLV320AIC3106. We are trying to connect the MIC 3R to HPLOUT our intention is Mic audio should be heard in speakers. 

I have shared the configurations below for the path. Mic to HPLOUT audio is still not heard.

please confirm us if the configuration is correct since audio is not heard in speakers.

Codec configuration:

Codec is master, sampling frequency is 48000 Hz 

Please reply at the earliest.

Regards,

Dilip

/* Page 0*/
WriteRegister(AIC3106_REG0_PAGESELECT, 0))

	/* Write software reset */
	WriteRegister(AIC3106_REG0_RESET, 0x80))
	

	/* N(ADC/DAC) = 1*/
	WriteRegister(AIC3106_REG0_CODEC_SAMPLE_RATE, 0x00))
	

	/* PLL disabled, Q = 2*/
	WriteRegister(AIC3106_REG0_PLL_A, REG_PLL_A_96KHZ))
	

	/* Write CODEC data path */
	WriteRegister(AIC3106_REG0_CODEC_DATAPATH, 0x0A))


	/* read back the CODEC data path */

	ReadRegister(AIC3106_REG0_CODEC_DATAPATH, &newValue))


	WriteRegister(AIC3106_REG0_ADDNL_GPIO_CONTROL_B, 0x01))	// CODEC_CLKIN uses CLKDIV_OUT



	ReadRegister(AIC3106_REG0_ADDNL_GPIO_CONTROL_B, &newValue))


	WriteRegister(AIC3106_REG0_CLOCK_GEN_CONTROL, 0x02))	// CLKDIV_IN/PLLCLK_IN uses MCLK, /2



	ReadRegister(AIC3106_REG0_CLOCK_GEN_CONTROL, &newValue))


	/* Audio Serial Data Interface A  */
	WriteRegister(AIC3106_REG0_SERIAL_DATA_INTFC_A, 0xF0))//BCLK,WCLK is output



	ReadRegister(AIC3106_REG0_SERIAL_DATA_INTFC_A, &newValue))


	/* Audio Serial Data Interface Control Register B */
	WriteRegister(AIC3106_REG0_SERIAL_DATA_INTFC_B, 0x00)) //IIS mode 16 bit word bit length,continuous transfer mode



	ReadRegister(AIC3106_REG0_SERIAL_DATA_INTFC_B, &newValue))


	/* Audio Serial Data Interface Control Register C */
	WriteRegister(AIC3106_REG0_SERIAL_DATA_INTFC_C, 0x08)) //IIS mode 16 bit word bit length,256 frame transfer mode



	ReadRegister(AIC3106_REG0_SERIAL_DATA_INTFC_C, &newValue))


	/* MIC3R --> Left ADC
	 * 		 |_> Right ADC
	 */

	/* AIC3106_REG0_LEFT_ADC_PGA */
	WriteRegister(AIC3106_REG0_LEFT_ADC_PGA, 0x00)) // PGA gain=0db


	/* AIC3106_REG0_RIGHT_ADC_PGA */
	WriteRegister(AIC3106_REG0_RIGHT_ADC_PGA, 0x00)) // PGA gain=0db


	/* AIC3106_REG0_LINE1L_LEFT_ADC */
	WriteRegister(AIC3106_REG0_LINE1L_LEFT_ADC, 0x7C)) //input 1 off, Left ADC powered up


	/*AIC3106_REG0_LINE1R_RIGHT_ADC*/
	WriteRegister(AIC3106_REG0_LINE1R_RIGHT_ADC, 0x7C)) //input 1 off, Right ADC powered up


	/* MIC3LR_LEFT_ADC */
	WriteRegister(AIC3106_REG0_MIC3LR_LEFT_ADC, 0xF0)) //MIC3L not connected and Mic3R is connected to Left ADC PGA


	/* MIC3LR_RIGHT_ADC */
	WriteRegister(AIC3106_REG0_MIC3LR_RIGHT_ADC, 0xF0)) //MIC3L not connected and Mic3R is connected to Right ADC PGA


	/* MIC3R MIC BIAS setting */
	WriteRegister(AIC3106_REG0_MICBIAS, 0x80)) 			//MICbias is powered down to 3.3 V,Digital MIC is enabled



	/* Mid Processing Block
	 * AGC is powered down,
	 */

	WriteRegister(AIC3106_REG0_LEFT_AGC_CNTL_A, 0x00)) 	// Left AGC disabled


	WriteRegister(AIC3106_REG0_RIGHT_AGC_CNTL_A, 0x00)) //Right AGC disabled


	WriteRegister(AIC3106_REG0_DAC_POWER_OUTPUT_DRVR, 0xE0)) // l/r DACs on, HPLCOM single-ended


	WriteRegister(AIC3106_REG0_HI_POWER_OUTPUT_DRVR, 0x10))  // HPRCOM single-ended

//#if 0
	WriteRegister(AIC3106_REG0_LEFT_DAC_VOLUME, 0x00))		// gain=0db


	WriteRegister(AIC3106_REG0_RIGHT_DAC_VOLUME, 0x00))		// gain=0db


	WriteRegister(AIC3106_REG0_DAC_L1_TO_HPLOUT, 0x80))		// DAC_L1 is routed to HPLOUT


	WriteRegister(AIC3106_REG0_HPLOUT_OUTPUT_LEVEL, 0x09))	// HPLOUT on


	WriteRegister(AIC3106_REG0_HPLCOM_OUTPUT_LEVEL, 0x00))	// 0db


aic3106codec.h

  • Hello Dilip,

    Since there is no straight path from MIC3R to HPLOUT, you need to use the PGA bypass path. I see that MIC3R is connected to both Left and Right PGA which is good. Registers 46 and 49 should be used accordingly to route the PGA outputs to HPLOUT. You have DAC_L1 routed to HPLOUT instead. 

    Regards,

    Aaron