Other Parts Discussed in Thread: TLV320ADC3101
Hello
I am working on developing a solution using TLV320ADC3101. So brought this EVM for testing. My current setup is to drive the I2S and MCK of the EVM from an external I2S master microcontroller(NRF52). I am using the 44.1Khz pre loaded image. From the microcontroller I2S clocks - BCLK, SCK and MCK is giving as input to the EVM.
Case 1:
Used on board mic and clock generated in the EVM. Via usb observed the audio recorded in audacity. Works very well.
Case 2:
Used on board mic and clocks generated in the external microcontroller. Via USB of the EVM observed the audio in audacity. It is a noise.Made sure the SW settings for Clock are OFF for I2S and MCK
MCK = 2.909MHz , BCK =1.454MHz , WS = 45.45KHz.
PLLCLKIN is configured as MCK.
P=1,R=1,K=32.0000,NADC = 2, MADC=8, AOSR = 128
Thus the clock ratio is equal to MCK*(1/64) = Sampling Freq
Is my approach correct ? How to use the evm to test externally generated clock?