For common component purposes, we want to use stereo speaker amplifier ICs for mono speakers as well.
Is this possible?
If possible, can I just fix one side of the IC to GND?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
For common component purposes, we want to use stereo speaker amplifier ICs for mono speakers as well.
Is this possible?
If possible, can I just fix one side of the IC to GND?
Hi,
Welcome to E2E and thank you for your interest in our products!
Do you refer to single-ended speakers? The output speaker drivers are independent from each other OUTR+/OUTR- are for one independent speaker and OUTL+/OUTL- are used for another speaker. Both outputs are used in a differential configuration. Since it is a Class-D driver, both outputs are required to be connected to the speaker. So, it is not possible to connect one side of the IC to GND.
Best regards,
Luis Fernando Rodríguez S.
Hi,
Thank you for the reply.
No, there is one differential speaker.
For example, OUTL+/OUTL- is connected to the speaker, but OUTR+/OUTR- is no connected.
And SDL is High, SDR is Low.
Is such a connection possible?
If it is possible, what happens to the INR+/INR- connection?
Hi,
Yes, this is the correct connection for a single channel mode.
Regarding the INR+/INR- connection, these pins should be connected to 0.1uF capacitors to GND when they are not used.
Best regards,
Luis Fernando Rodríguez S.