This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SRC4190-Q1: Can be used with PCM1754-Q1?

Part Number: SRC4190-Q1
Other Parts Discussed in Thread: PCM1754-Q1

Hello Team,

Customer want to use SRC4190-Q1 and PCM1754-Q1

Q. Is there any problem if they use the combination of SRC4190-Q1 and PCM1754-Q1?

Q. Is there example block diagram or reference circuit of SRC4190-Q1+PCM1754-Q1?

Thanks,

Yuta Kurimoto

  • Hi Yuta,

    At a high level, there is no problem using a sample rate converter with a DAC. I'm not aware of any reference designs with these two devices. If you have any specific questions about using the two devices let us know!

    Best,

    Zak