Hello Experts,
I have couple of question for TPA3220. Would you please answer them?
1. RESET
The datasheet mentioned below comment.
"To ensure thermal reliability, the rising edge of RESET must occur no sooner than 4 ms after the falling edge of FAULT." Why 4ms wait time is needed? Would you please explain more detail?
2. OSCP, OSCM connection
If I would like to use TPA3220 in master mode and only one device is used, how can I connect OSCP and OSCM terminals? These terminals should be floating, correct?
3. Table 5 in datasheet
What does "A,B,C,D" mean? My understanding is it means an each of half bridge as follows. Is my understanding correct?
A => OUT1_P
B => OUT1_M
C => OUT2_P
D => OUT2_M
4. /FAULT, /OTW_CLIP
Regarding a following thread, when can you update the datasheet?
https://e2e.ti.com/support/audio/f/6/t/738592?tisearch=e2e-sitesearch&keymatch=TPA3220%2520fault
Best Regards,
Fujiwara