Part Number: PCM4222
Other Parts Discussed in Thread: OPA1632
Hi,
I am implementing the PCM4222 in a design and i have a question in respect to the maximum analogue input voltage on pins VinL+/VinL- and VinR+/VinR- for FSD.
The datasheet states on page 5 that the full scale voltage is 5.6v pk-pk differential input. This is repeated on page 17 too.
With VCOML/VCOMR at 1.95volts, and the OPA1632 used as the differential output opamp for the input circuit as per page 31, then the stated full scale input is stated to be 2.8v pk-pk as per page 5 and page 17, described as per pin.
Figure 37 on page 17 shows that the input voltage range is 2.8v pk-pk centred on a mean DC of 1.95volts. This translates to a minimum input voltage 0.55volts to a maximum input voltage 3.35volts to achieve 2.8volts pk-pk.
Therefore, how is it that a 5.6volts pk-pk is possible as a differential input voltage, if the Vcc analogue supply is +4volts ?.
This would mean that the analogue input voltage is 0.75volts greater than the Vcc supply, or 0.85volts lower than analogue ground.
As such, what is the correct differential voltage across the pins VinL+/VinL- and VinR+/VinR-, to achieve FSD ?
Thanks and regards,
Shadders.