Hi All,
There is a same issue of some Components. In Audio codec IC, There is no voltage at Speaker output (spkp1,spkM2,spkp2,spkM2). I have checked with following commands:-
And found that In register 37,the 4th bit is not changing there value and it's shows class-D driver is not Powerup according to datasheet, & I2C,I2S ,BLCK,DAC_DIN, WLCK Communication with Processor is running fine . I have checked ,Pin Spkp1 with respect to ground It's shows 0V. but in good audio IC found that Spkp1 with respect to ground is 2.5V.
I have attached Schematic of Audio IC & Register Configuration.
Page 0 0 1 2 3 4 5 6 7 8 9 a b c d e f 0123456789abcdef 00: 00 00 01 66 03 91 08 00 00 00 00 82 88 00 80 80 ..?f???....??.?? 10: 08 00 01 01 80 80 04 00 00 00 81 00 00 00 01 00 ?.?????...?...?. 20: 00 00 00 00 80 88 11 00 00 00 00 00 00 00 00 00 ....???......... 30: 2c 00 00 17 32 12 02 02 02 11 10 00 01 04 00 d4 ,..?2??????.??.? 40: 00 ec 00 00 2f 38 00 00 00 00 00 ee 10 d8 7e e3 .?../8.....???~? 50: 00 00 80 00 00 00 00 00 7f 00 00 00 00 00 00 00 ..?.....?....... 60: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................ 70: 00 00 00 00 00 02 00 00 00 00 00 00 00 00 00 00 .....?.......... 80: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................ 90: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................ a0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................ b0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................ c0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................ d0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................ e0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................ f0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................ Page 1 0 1 2 3 4 5 6 7 8 9 a b c d e f 0123456789abcdef 00: 01 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ?............... 10: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 04 ...............? 20: 06 3e 00 40 74 7f 80 7f 02 02 1c 00 20 86 00 80 ?>.@t??????. ?.? 30: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................ 40: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................ 50: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................ 60: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................ 70: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................ 80: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................ 90: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................ a0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................ b0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................ c0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................ d0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................ e0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................ f0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................