Hi,
I wanna use PCM1754 to drive TPA2008D2, there are some problem when i am designing the circuit
you know,PCM1754 have two chanels analogy output and TPA2008D2 has two differential audio inputs.How to connect the signal? I mean i connect one analogy source to the INP input and ac groud INN input through a capacitor . The INN input also need to connect VCOM pin from PCM1754.Is it right?
Thanks
Devin