Part Number: PCM1690-Q1
Hello Team,
PCM1690-Q1 has Pin19(AMUTEO), Pin20(MD/SDA/DEMP). These are open-drain output with active low.
Q. Does these pin have internal pull-up resistor? or do we need to add external pull-up resistor?
If these pin has internal pull-up resistor, I want to ask one more question as below.
Q. For Pin20, If not I2C mode, this pin behaves input pin as MD, DEMP. In this case the internal pull-up register still active?
Thanks,
Yuta Kurimoto