Dear All,
In TPA3110D2 spec sheet, there is a description of necessary slew rate of gain setting pins as below:
9.3.2 Gain Setting Via GAIN0 And GAIN1 Inputs
The gain of the TPA3110D2 is set by two input terminals, GAIN0 and GAIN1. The voltage slew rate of these gain terminals, along with terminals 1 and 14, must be restricted to no more than 10V/ms. For higher slew rates, use a 100kΩ resistor in series with the terminals.
Please let me know why digital setting pins of GAIN0 and GAIN1 has slew rate indication?
How does rising-up time affect the gain setting function?
Best Regards,
Andy