Other Parts Discussed in Thread: PCM1795, SA5534, SA5532A, NE5534, , NE5532
Hi team,
Customer want to use SA5534 or SA5532A as I/V conversion for PCM1795.
PCM1795 recommend NE5534 but they choose SA5534 because wider temperature range is necessary.
Could you comment we can use SA5532A (2ch) instead of SA5534A (1ch)?
SA5532A can achieve smaller PCB area and lower price so I would use this device if possible.
About NE5532, Icc is 8mA (typ) when Vo=0, no load.
Is NE5532 able to output 8mA each channel or both channel?
Best regards,
Koyo