Other Parts Discussed in Thread: PCM1795, , OPA1678, TL974, OPA1679, SA5532
Hi team,
This is very urgency question because customer have to fix a device for I/V transition of PCM1795 due to AKM issue.
Could you please help to answer ASAP?
Their specification is that power is +8V/GND and center voltage at output is +2.5V.
The output of PCM1795 will be 4mA pk to pk and they want to swing with 2.8V pk to pk.
Is SA5532A rail to rail input/output?
I don't think this is rail to rail because this device is bipolar structure and following spec shows 2V at upper side and bottom side can't be used.
Is my understanding correct?
How about input rail?
I would like you to inform this device can achieve their specification.
Best regards,
Koyo