This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320ADC3100: Need example for how to initialize TLV320ADC3100

Part Number: TLV320ADC3100

Hi 

Can you help share an example for TLV320ADC3100  initialization 

below is our configuration

1. Single end Left channel audio line in from IN2L(P)  pin 7

2. Single end Right channel audio line in from IN2L(P)  pin 7

3. IN3L(M) and IN3R(M) no used, 0.47  uF connect to ground 

4. MCLK input 12.288MHz

5. TLV320ADC3100  work in I2S slave mode with 

     WCLK = 48KHz input  (we are feeding LR CLK to WCLK)

     BCLK =  3.07299 MHz (64 fs)

     24 bit data