Could you pls provide the detailed information of PCM1793 as below:
1. ESD level
2. reflow times
3. IBIS model
4. the requirements for solderability
5. thermal parameters Tc、Tj、Ta、θjc、θja
6. MP date
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Could you pls provide the detailed information of PCM1793 as below:
1. ESD level
2. reflow times
3. IBIS model
4. the requirements for solderability
5. thermal parameters Tc、Tj、Ta、θjc、θja
6. MP date
Hi James,
1. HBM ESD - HBM 2000 V
2. I have requested this information
3. There is no IBIS model for this device.
4. I have requested this information
5. I have requested this information
6. The device was released in March 2003.
Thanks,
Paul
1. HBM ESD - HBM 2000 V
2. This device was compliant with the JEDEC standard at the time of qualification: IPC/JEDEC J-STD-020C
3. There is no IBIS model for this device.
4. This device was compliant with the JEDEC standard at the time of qualification: IPC/JEDEC J-STD-020C
5. The thermal information has been requested, but it usually take a few weeks to get the report.
6. The device was released in March 2003.
IPC/JEDEC J-STD-020C