Please tell me about the start and end sequences.
I am thinking of starting and terminating by Power-On Reset.
According to the data sheet P.81, after the voltage value of the internal LDO is 1.5V and the [LDO_GOOD] flag is set to High, the clock is digitally reset with 16 pulses.
Please tell me the threshold voltage of Power-On reset.
DVDD: __V
AVDD: __V
IO VDD: __V
How many seconds below the threshold to reset?
time:
[As a condition]
-Do not input MCLK and use the internal PLL from BCK.
-The INT pin is pulled down with 10kΩ.