Hello Experts,
I would like to understand a definition of input voltage spec. The datasheet specified VIN(max)=+/-2.8V. My understanding is that the maximum input voltage swing is -0.3V~+5.3V (VDD=5V, per INx_P/M), correct?
Best Regards,
Fujiwara
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Experts,
I would like to understand a definition of input voltage spec. The datasheet specified VIN(max)=+/-2.8V. My understanding is that the maximum input voltage swing is -0.3V~+5.3V (VDD=5V, per INx_P/M), correct?
Best Regards,
Fujiwara
Hi Fujiwara-san,
Yes, you are correct.
There is additional information on page 5 of datasheet, that the input pins Abs max range is -0.3-5.5V.
Thanks!
Regards,
Sam