Hi,
We need to input "common audio clock" to enable "Clock Divider Autoset".
Is "common audio clock" shown values at "13.1.2 PLL Tables for Software Controlled Devices" on the datasheet?
Best Regards,
Kuramochi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We need to input "common audio clock" to enable "Clock Divider Autoset".
Is "common audio clock" shown values at "13.1.2 PLL Tables for Software Controlled Devices" on the datasheet?
Best Regards,
Kuramochi
Hi Kuramochi-san,
If you are using the auto-set functions, you should use one of the clock combinations from Table 32 "System Master Clock Inputs for Audio Related Clocks". If, for example, if you used an LRCK of 24kHz (which is not on the table), you would need to disable the auto set functions and manually set the clocks based on the "PLL Tables for Software Controlled Devices".
Thanks,
Paul