Hi
My customer is noticing that in a design they have the LM386 has a noise (hissing) on the output when there is a steady input of +1.8V on pin 3. The customer came across a website stating that if he grounds pin 7 (BYPASS pin) instead of using a 10uF cap, this will mute the output and eliminate the noise. He is planning to add a mux to pin 7 either connect 10uF (in normal operation) or ground it in speaker off condition.
Another point the webpage he looked at made was that the inverting input is less noisy than the non-inverting input.
Can you confirm if this is ok to do and provide any other recommendations?
Thanks,
Jose