Other Parts Discussed in Thread: PCM2903C, , PCM2903
Dear Specialists,
My customer is considering PCM2903C and confirming PCM2903EVM-U.
Could you please advise about their question.
---
I would like to evaluate the IC of PCM2903C.
It is confusing because the description in the product folder of PCM2903EVM-U and the description in the user guide are different.
Could please advise which one is correct.
(1) In the description of the PCM2903EVM-U product folder, PCM2903C is used.
(description)
The PCM2903EVM-U is an evaluation module for the PCM2903C USB audio codec.
The EVM is supported by Windows® XP, Windows® Vista, Windows® 7, OSX and most operating systems which are compatible with USB class audio devices.
The PCM2903EVM-U connects to a USB port of a PC. The USB interface provides power, control and streaming audio data to the EVM.
- Full-featured evaluation module for the PCM2903C audio codec.
- USB connection to PC provides power, control, and streaming audio data for easy evaluation
(2) According to the PCM2903EVM-U User's Guide, PCM2903 (NRND) is listed.
(description)
The PCM2903EVM-U is an evaluation board for Texas Instruments' newly developed USB interface codec, PCM2903.
The PCM2903EVM-U evaluation module (EVM) includes a PCM2903.
It is a self-powered USB codec without an S/PDIF interface.
(3) If PCM2903 is used, are there any restrictions due to the difference from PCM2903C?
---
I appreciate your great help in advance.
Best regards,
Shinichi