Hi team,
Could you advise the accuracy (tolerance) of the MICBIAS at 9V?
Load regulation is specified at max 1%, but I would like to know the accuracy.
regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Could you advise the accuracy (tolerance) of the MICBIAS at 9V?
Load regulation is specified at max 1%, but I would like to know the accuracy.
regards,
Hi Zak,
I would like to know the accuracy(tolerance) to know the range of input overvoltage detection voltage.
Since it is referred to MICBIAS voltage, I would like to know its tolerance.
regards,
Hi Shinji-san,
The accuracy of MICBIAS is much better than the threshold settings so this should not be a major concern. This is also dependent on the actual MICBIAS setting used and we don't have any specs for this, but as a worst case estimate I would expect the MICBIAS to be within 20mV of the set voltage.
Best,
Zak