Other Parts Discussed in Thread: TAS5825PEVM, TAS5825P
Hello,
I just start my work on the TAS5825PEVM and PurePath Console 3. I'm trying to understand the header file export and the extravagent large number of register to be written.
I got most of the book 0 / page 0 ones which are describe in the datasheet. I got some of the book 0x78 (level meters), book 0x8C (DRC, Volume Alpha, etc..) and 0xAA (BQ) which are mentionned in the slaa786a.pdf. But I got no clue about all the rest like book 0x78 or book 0x64 or even book 0xAA page 0x0E which is not mentionned elsewhere.
Well in brief I really want to know what I really need to write and what is pure default overwritting generated by PPC3... as writing 6000+ bytes seems a little bit overkill and time consumming if it's not needed. But as an extanded question is there a complete description of book, page and register for the TAS5825P that we can access ?
Sincerely
Sylvain GARNAVAULT
PS : PPC3 prompt a warning when connecting the EVM where it claim a device id of 0x97 which should not be possible so I suspect a bug here and it's part of triggering my suspicion about what PPC3 really generate properly or not...