Hi,
According to the datasheet, I can set the GPIO1 as "SDOUT2", so I can use two I2S interfaces.
Now I want to use 4 channels(4 Dmic or 2 Amic+2 Dmic), then I only need to use Slot 0 and Slot 1.
Is the I2S interfaces can only output Slot 0 and Slot 1 In this situation? (do not need Slot 3, Slot 4 .......)
BR
Frank