This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM1860-Q1: Making high resolution DC & AC measurements using an 24 bit Audio converter

Part Number: PCM1860-Q1


My customer is wondering whether it is possible to use a 24bits audio converter for thin DC & AC measurements?

For example, can the 24bit/192kHz adc, ref PCM1860QDBTRQ1 make high resolution DC & AC measurements?

Some questions come to mind:

  • Sampling can be achieved nearly simultaneously on 2 channels at the same time, at 192kHz/24 bits :
  • Can the sampling frequency changed to others values than the one given in the datasheets : example setting it to 100kHz, 50kHz…?
  • Does the sampling is simultaneous on 2 channels (1 way left-right)? What is the jitter?
  • Does the bandwidth include DC voltage?
  • What is the precision I can expect with DC sampled voltage?
  • What will be the rms noise with a flat gain (0dB)
  • As signal treatments achieved with raw datas thanks to uP, which digital link can be used to get them?

Thanks

Josef

  • Hi Josef,

    To answer your questions:

    • Sampling can be achieved nearly simultaneously on 2 channels at the same time, at 192kHz/24 bits :
      • Yes, there are 2-4 separate ADC in the device that will run at the same rate so the sampling happens simultaneously. 
    • Can the sampling frequency changed to others values than the one given in the datasheets : example setting it to 100kHz, 50kHz…?
      • In general yes this should be supported but will require custom configuration and we would need to verify any non-audio rate works correctly as this is not the intended use-case.
    • Does the sampling is simultaneous on 2 channels (1 way left-right)? What is the jitter?
      • Sampling is simultaneous but we don't have a spec for phase between the two but it should be very similar. Channel matching is quite good.
    • Does the bandwidth include DC voltage?
      • A HPF is enabled by default but can be disabled.
    • What is the precision I can expect with DC sampled voltage?
      • Audio devices are not trimmed for DC precision so the DC accuracy is not likely to be very good and will vary between devices. Accuracy is only trimmed to 0.5dB.
    • What will be the rms noise with a flat gain (0dB)
      • This is given by the SNR spec. Roughly 13.3uVrms.
    • As signal treatments achieved with raw datas thanks to uP, which digital link can be used to get them
      • I'm not sure I understand this question. The device supports I2S, TDM, and LJ output formats

    Best,

    Zak