Part Number: OPA1692
Hello,
According to the Figure 13. Maximum Output Voltage vs Frequency of OPA 1692, we could get to the conclusion about the output amplitude is more than 4Vp when the Frequency less than 1Mhz with +-5V,2Kohm load. So if the power supply is 8V, and the load is decreased to 1Kohm, does it the output amplitude get to 4Vrms(5.66Vp)?Our customer want to select one audio amplifier which need to get to 4Vrms output with 1Kohm load. I think the OPA1692 could meet his need. Do you have any other opinions?
Best regards
Kailyn