Dear expert,
the PPS process flow do not work after upgrading the sampling frequency from 24K to 22.05K, it seems like the dsp register do not write successfully, the time waveform is not correct as expected in the process flow, for example, there is an absolute block in the right output, but the timewave in the right channel do not turn up in the Audacity display, could you pls help to identify what is the reason?
the PPS can work properly before upgrading, I don't know what else should I take care of?
Remark: the downloading result is successful after clicking the "Build"--->"downloading and run" , and no error comes out. and also the ADC3101 CS can also recognise the EVM board
is there any specialized USB driving package for the EVM?
the PPS code is as below:
;IADC = %%prop(miniDSP_A_Cycles);
reg[47][95]=0x00
reg[47][96]=0x00
reg[47][97]=0x00
reg[0][1]=0x01
reg[0][61] = 0x00 ; reg(0)(0x3d => 61) ADC ADC prog mode
reg[0][4] = 0x03 ; PLL_CLKIN = MCLK, CODEC_CLKIN=PLL_CLK
reg[0][5] = 0x91 ; P=1, R=1
reg[0][6] = 0x08 ; J=8, settings are for fs = 44.1khz
reg[0][18] = 0x84 ; reg(0)(0x12 => 18) ADC Powerup NADC = 4, mkmkmk add an additional divide by 2 vs 3254 since only 512 instructions available
reg[0][19] = 0x84 ; ADC Powerup MADC = 4
reg[0][27] = 0x00 ; reg(0)(0x1b => 27) Mode = i2s & wordlength = 16
reg[0][20] = 128 ; reg(0)(0x14 => 20) ADC AOSR = 128
reg[0][83] = 0x0 ; adc vol control = 0db
reg[0][84] = 0x0 ; adc vol control = 0db
reg[0][22] = 4 ; Decimation Ratio = 4
reg[0][21] = %%eval(%%prop(miniDSP_A_Cycles)/2) ; IADC
PROGRAM_MINIDSP_A
reg[1][52] = 0xfc ; reg(1)(0x34 => 52) ADC IN1_L is selected for left P
;reg[1][54] = 0x3c ; reg(1)(0x36 => 54) ADC CM1 is selected for left M
reg[1][55] = 0xfc ; reg(1)(0x37 => 55) ADC IN1_R is selected for right P
;reg[1][57] = 0x3c ; reg(1)(0x39 => 57) ADC CM1 is selected for right M
reg[1][59] = 0x00 ; reg(1)(0x3b => 59) ADC unmute left mic PGA
reg[1][60] = 0x00 ; reg(1)(0x3c => 60) ADC unmute right mic PGA
reg[0][81] = 0xc2 ; reg(0)(0x51 => 81) ADC Powerup ADC left and right channels (soft-stepping disable)
reg[0][82] = 0x00 ; reg(0)(0x52 => 82) ADC Unmute ADC left and right channels