TA = 25°C, AVDD = 3.3 V, IOVDD = 3.3 V, fIN = 1-kHz sinusoidal signal, fS = 48 kHz, 32-bit audio data, BCLK = 256 × fS, TDM slave mode, PLL on (unless otherwise noted)
IN1 differential input selected and AC signal shorted to ground, DRE enabled (DRE_LVL = –36 dB, DRE_MAXGAIN = 24 dB), 2.5-kΩ input impedance selection.
It is best to measure the noise floor with the differential inputs shorted together and AC coupled to GND.
with this test condition,the snr value not achieve 120db,it's 110db,