This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3109EVM-K:

Part Number: TLV320AIC3109EVM-K
Other Parts Discussed in Thread: TLV320AIC3104-Q1

Hi Team,

Now I'm trying to test TLV320AIC3109EVM-K in WINDOWS 10 OS base.
Successfully installed AIC310x GUI and updated NI VISA, but failed to install USB device driver as below.
I'm not sure it needs Administrator right to install the driver but it's lock to install it by TI policy?

Tried to install at USB-MODEVM with USB-MODEVM_vista&7.inf, USB-MODEVM_WDM.inf  files several times but failed, and also can't detect it at GUI(TLV320AIC3104-Q1) too.

Please let me know how can install USB driver?

  • Hello Lenny,

    Apologies for the delay on this. I have just returned to the office. 

    There are several other things that I would like to check here. The first is making sure that the Windows driver signature enforcement was disabled during the installation of the drivers. Can you confirm if this Windows feature was disabled? If not, I recommend disabling this feature and installing the necessary drivers by doing the following:

    1. Go to Windows Settings

    2. Click on Update & Security

    3. Go to Recovery tab on the left

    4. Go to Advanced startup and restart the PC

    5. Then go to Troubleshoot --> Advanced Options

    6. On the bottom of the window, click on See More Recovery Options

    7. Start-Up settings --> Restart

    This should disable the driver signature for windows and restart your PC. You can then re-install the drivers after your PC reboot. Let me know if this helps. 

    The second thing I would like to check here is the SW-2 settings. I see that you linked a previous post that discusses this. Were you able to confirm that SW-2 is in the correct position? If you provide a picture, I can take a look and confirm. 

    Regards,

    Aaron Estrada