See attached schematic of LME49724, with dc servo circuit to null dc offset voltage on the outputs.
The input to the LME49724 is the summation of two signals.
Note: I realize that I should add another 0.1uF cap across R55 (so it is the same as R54).
- Is this the correct way to implement a dc servo with the LME49724?
- Is there a better choice of part to use for the dc servo than the LT1097S8?
Thank you