- the speaker is rated for 3W and its impedance is 8ohm.
- with a 12V VBAT.
- the DVC_PCM is set to -30 dB
- the amplifier level to 21dBV.
The issue is when I increase the PCM volume above -20dB, TAS2770 shuts the PWM off. It does not recover until the board is rebooted, even if the volume is lowered.
Please help me to solve this issue.