Hi All,
My customer intend to use the LM48580 and have below questions:
1. Is VOUT+/-(VBST) voltage adjustable?
2.Based on the spec, may i confirm that the Vp-p are +15V and -15V?
Thank you for your help.
Best Regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi All,
My customer intend to use the LM48580 and have below questions:
1. Is VOUT+/-(VBST) voltage adjustable?
2.Based on the spec, may i confirm that the Vp-p are +15V and -15V?
Thank you for your help.
Best Regards
Hello,
You can adjust the GAIN pin which will have an impact on VOUT+/-.
Yes. That is correct. You can also look at the application curves (figures 16 and 17) for reference.
Best Regards,
Justin Beigel